Cancel
Showing results for 
Search instead for 
Did you mean: 

NX8.5, G-code file simulation, TURNING, 3d material removing

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

My customer have NX8.5, and want to simulate G-code file, turning. No 3d material removing.

NX8.5.3.3, maintenance pack 09  

No way to solve this problem in NX8.5?

1 REPLY 1

Re: NX8.5, G-code file simulation, TURNING, 3d material removing

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

It works from version NX9.0. In NX8.5 IPW for turning operations and milling operations - are two different IPW, material removal in turning operations in the simulation program from the file did not work and can not pinch chuck until it touches the turning IPW.

Learn online





Solution Information