Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

NX9 Face Mill Cutter option is not available

Experimenter
Experimenter

Not able to create face mill cutter in NX 9.0.3 MP11 when creating from Create New Tool.

It is avalilabe in NX7.5.

TC10 NX9 + BCT16 Platform
1 REPLY 1

Re: NX9 Face Mill Cutter option is not available

Use the Chamfer Mill create the face mill shape.

 

Before NX 8.5, the Face Mill subtype just created an end mill with corner radius. This is not accurate whenthe cutter has a chamfer, so it was removed and the Chamfer Mill was added.

 

Face Mills in the tool library are mapped to Chamfer Mills when retrieved.

Mark Rief
Retired Siemens

Learn online





Solution Information