Cancel
Showing results for 
Search instead for 
Did you mean: 

NX9 Mill Slot on OD

Experimenter
Experimenter

Can anyone help how I can mill the slot on an OD?

The machine only has capability to use the X, Z & C axis so with the slot being 6mm then the cutter is size for size with the slot.

Required code:

G00 X50.0 Z-30.0 C0.0

X12.5

G01 X7.5

C-90.0

Z-10.0

X12.5

X50.0

 

Shaft.PNG

Thanks

5 REPLIES 5

Re: NX9 Mill Slot on OD

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Should be possible with Generic Motion operation

https://community.plm.automation.siemens.com/t5/Tech-Tips-Knowledge-Base-NX/How-to-use-Generic-Motio...

 

Marek Pawlus, NCmatic

Development: C#, Tcl/Tk, CSE

Re: NX9 Mill Slot on OD

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

And (possibly) variable axis, tool axis "away from line" (CL of the part), swarf cutting

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: NX9 Mill Slot on OD

Legend
Legend

like Marek and Ken said, here are two of the possible solutions

have a nice day

ciao

 

Re: NX9 Mill Slot on OD

Legend
Legend

Nice example. I'm saving this for future reference

 


Dennis Rathi
Creations Unlimited

Re: NX9 Mill Slot on OD

Experimenter
Experimenter

Thanks for that.

Will use that one

Learn online





Solution Information