Cancel
Showing results for 
Search instead for 
Did you mean: 

[NXCAM] Nutating CA/CB Head Setup - OFFSET

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi Experts,



Perhaps some of you have already met on 5-axis machine with a head having offset (axis).
Trying to create a procedure in Post Builder, which will allow the rotation offset correction 4 and 5 axis.

Head_HSD.jpgIf you have a procedure which could be adapted to your case or written postprocessor with such a solution, please write.

Machine: Haltron4 (Fanuc - XYZCA)
 

Thanks,

Grzegorz Kozlowski
Cador Consulting Sp. z o.o. (Poland)
601 150 761
3 REPLIES

Re: [NXCAM] Nutating CA/CB Head Setup - OFFSET

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I'm not sure I understand what you're asking...

Is this a 5 axis head that can be added to a 3 (or 4 or 5) axis mill?

Or is this a permanent set up (i.e. rotary axes are always present)?

 

 

1) Added when needed case

Set up a separate 5 axis post & link to main.  Use Method /"Head" UDE tto switch posts.

 

2) Permanent

In the fourth/fifth axes pages of the "machine tool" view, just set up appropriate offsets.

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: [NXCAM] Nutating CA/CB Head Setup - OFFSET

Phenom
Phenom

It is best to have the control handle head and tool compensation. For Fanuc - that is G43.4. If that is not an option - I am not aware of out of the box code to throw an offset for a twist head. There are (however) math routines to help.They can be found in ugpost_base.tcl in the POSTBUILD\pblib directory - this file is souced in for every PB post.

NX10.03
Windows 7 Pro

Re: [NXCAM] Nutating CA/CB Head Setup - OFFSET

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Guys,

 

Thank you for your suggestions.
If necessary, I have a problem that you have to ask for help.

 

Regards,

 

Learn online





Solution Information