Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

[NXCMM] Interferece check interpolating path between some operations.

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

NXCMM is able to do interference check each operation path,
but it isn't able to do same check imterpolating path between two operations.

 

If I would like to try interferece check imterpolationg path,but I don't know how to do that.

If someone knows how to do that, could you tell me please.

2 REPLIES 2

Re: [NXCMM] Interferece check interpolating path between some operations.

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

When running machine simulation with collision checking on, all motion of the probe is accounted for including between each path operation. The best thing to do is to simply simulate the entire program by highlighting the "CMM_INSPECTION_PROGRAM" group, right mouse click and select simulate. This works as long as you have a machine, head and tool defined.

 

In NX 10.0.3 we are also adding a visualization aid (green dashed lines) that shows the path of the probe between inspection paths

Re: [NXCMM] Interferece check interpolating path between some operations.

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

To:sciggy87

 

Thank you for your commnet!
Certainly you said, using machine simulation I can confirm interpolating path
and detect inteference.

 

But if possible, I thought I would like to check interpolating path
without running operations.
because customer want to do. They said

 

" If all path (including interpolating path) are displayed
  then it is easy way to check path roughly
  Certainly, simulation is able to check all path
  but we hope to check all path easily"

 

>In NX 10.0.3 we are also adding a visualization aid (green dashed lines)
> that shows the path of the probe between inspection paths

 

I think "NX 10.0.3 new function you said" match above customer's hope.
I'm looking forward to try in NX10.0.3!

 

Thanks a lot.

 

Mosu

Learn online





Solution Information