Cancel
Showing results for 
Search instead for 
Did you mean: 

Nearest neighbour interpolation behaves like it is linear interpolation in NX acoustic

Creator
Creator

I am trying to use an acoustic monopole source with the power as in the attached figures.
However, when I run a simulation with this it behaves like it is using linear interpolation instead. The small difference is due to the fact that the nearest neighbour simulation had a source input at 201Hz instead of at 200Hz. 
I am using SImcenter 3D.

Is this a bug or am I missing something.

3 REPLIES 3

Re: Nearest neighbour interpolation behaves like it is linear interpolation in NX acoustic

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I'm thinking this would be better asked in one of the Simcenter forums?

This forum (NX Manufacturing) is for NC programming, additive manufacturing, and related topics...

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Nearest neighbour interpolation behaves like it is linear interpolation in NX acoustic

Phenom
Phenom

Wrong forum. Linear interpolation has a different meaning here. Smiley Very Happy

 

 

good-glavin.jpg

Glenn Balon
Production: NX 12.0.2 MP10 Primarily CAM

Re: Nearest neighbour interpolation behaves like it is linear interpolation in NX acoustic

Creator
Creator

I have asked the question on the simcenter forum now.

Learn online





Solution Information