Cancel
Showing results for 
Search instead for 
Did you mean: 

New Tap Cycles

Genius
Genius

I recently updated to NX9.0.3, and noticed there are new tap cycles in the hole_making operations, but in Postbuilder I'm not seeing any areas to define output for these new cycles. Are these just place holders for future functionality or do I have to create my own User Defined Cycles?

Mike Diamond, CNC Programmer, Orizon Aerostructures Inc.

Production: NX10.0.3.5, Vericut 8.1.4, ICAM V21
Development: VB.NET, Tcl/Tk
Testing: NX12
3 REPLIES 3

Re: New Tap Cycles

Siemens Legend Siemens Legend
Siemens Legend

The new tap-float, tap-deep & tap-breakchip cycles should be available when you create a post using Fanuc 30i, Fanuc 30i Advanced, or Semens 840D template post as the seed.

Re: New Tap Cycles

Genius
Genius

How does one add them to the existing posts?

Re: New Tap Cycles

Siemens Legend Siemens Legend
Siemens Legend

It would require mocking the PUI file to enable the upgrade from one of the controller posts. Outcome is NOT warranted.

Learn online





Solution Information