Cancel
Showing results for 
Search instead for 
Did you mean: 

New features in 9.0.3.mp01, cannot see new check boxes flow cut operations.

I am running 9.0.3 mp01 and do not see the check boxes for center passes in flowcut operations.  The docs say the check boxes are in the non-steep and steep groups of the flowcut drive method dialog.

 

Is there an env variable that is needed?

NX 12.0.2
1 REPLY

Re: New features in 9.0.3.mp01, cannot see new check boxes flow cut operations.

I just noticed the center pass option is available for follow periphery cut pattern, not other cut patterns.

NX 12.0.2

Learn online





Solution Information