Cancel
Showing results for 
Search instead for 
Did you mean: 

New work instruction features -- THANK YOU Developers

Legend
Legend

Logged in tonight and saw this new tech tip! Been asking for something like this since 8.5 when I learned the limitation of excel shop docs.

 

For those of you who haven't seen this new feature yet..

 

http://community.plm.automation.siemens.com/t5/Tech-Tips-Knowledge-Base-NX/Eliminate-errors-with-bet...


Dennis Rathi
Creations Unlimited
31 REPLIES

Re: New work instruction features -- THANK YOU Developers

Legend
Legend

Good One !

Re: New work instruction features -- THANK YOU Developers

Experimenter
Experimenter
I have the latest NX10 up date but I don't see the work instruction selection.

Re: New work instruction features -- THANK YOU Developers

Valued Contributor
Valued Contributor

I cannot see it either, the video is too small in window to see what is happening and too blurred at full screen to see how you start the process

 

NX10.0.2.6

Mike

NX 11.0.2.7
Win 10

Re: New work instruction features -- THANK YOU Developers

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I have 10.0.2 (no MP) installed.

if I look in the mach\resource\template_part\english (or metric) I see

work_instruction.prt

 

But it isn't used in any of the \template_set\ *.OPT files.

 

- could be in a 10.0.2 MP

- could be its coming in 10.0.3

 

If I "browse" to it I see only 1 operation type to add (not 2 per the video)

 

I see no "right click" action either...

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: New work instruction features -- THANK YOU Developers

Work instructions will be released in NX 10.0.3.

 

The video tech tip was done as a preview in 10.0.2. We'll change the text to make that clear.

Mark Rief
Retired Siemens
Highlighted

Re: New work instruction features -- THANK YOU Developers

Legend
Legend

When does it come out?

 


Dennis Rathi
Creations Unlimited

Re: New work instruction features -- THANK YOU Developers

Valued Contributor
Valued Contributor

Saw this as well and it loks great!

@MarkRief Can these tech tips videos be presented in future at higher defiinition? Going full screen on 2560x1440 or even a 1680x1050 monitor completely destroys legibility. Forget about it on a high DPI monitor!

 

Its the one downfall about what is some excellent material.

Re: New work instruction features -- THANK YOU Developers

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The unofficial date for 10.0.3 (that I've seen) is Nov 17, 2015.  It could be a couple days either way. Usual disclaimers apply (particularly since I'm not a Siemens employee)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: New work instruction features -- THANK YOU Developers

Regarding the video, we are aware of this issue with the blurry video. The original video is actually very good resolution, but the site is making adjustments that affect the resolution. We are still trying to resolve this. 

 

As a workaround, in the 10.0.2 articles we started to add links to download the videos locally. I'll see if we can do the same for this one.

Mark Rief
Retired Siemens

Learn online





Solution Information