Cancel
Showing results for 
Search instead for 
Did you mean: 

Non cutting moves

Builder
Builder
How change non cutting moves of already generated toolpath without generating twise???
8 REPLIES 8

Re: Non cutting moves

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

in NX it is called Smart Regeneration

 

documentation says:

 

"Generating non cutting moves only

You can generate only the non cutting moves that you change in an operation without regenerating the entire tool path.

  • To enable this functionality, set the Do Smart Regeneration when Possible customer default or manufacturing preference.

  • You must generate the operation first in order to create the data necessary for the Smart Regeneration.

  • The non cutting moves that you can generate using Smart Regeneration are limited to engage, retract, and transfer.

  • If you modify any parameters other than the non cutting moves, the full tool path will be regenerated."

Marek Pawlus, NCmatic

Development: C#, Tcl/Tk, CSE

Re: Non cutting moves

Builder
Builder
Where is this option ?

Re: Non cutting moves

Builder
Builder
Im not able to find this option in nx

Re: Non cutting moves

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

which NX version do you use?

 

You can't find Customer Defaults?

it is in File --> Utilities --> Customer Defautls

Marek Pawlus, NCmatic

Development: C#, Tcl/Tk, CSE

Re: Non cutting moves

Builder
Builder
Nx 10.0.0.24

Re: Non cutting moves

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

so you need to install latest updates

Marek Pawlus, NCmatic

Development: C#, Tcl/Tk, CSE

Re: Non cutting moves

Builder
Builder
Ok

Re: Non cutting moves

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

In 10.0.3.5 MP19 customer defaults it is under Manufacturing -> Operation -> "Tool Path" tab

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information