Cancel
Showing results for 
Search instead for 
Did you mean: 

Not get I J and K values.

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hello,

I J K value are missing in my NC output. i have forced out these commands in motion/circular move. then too they are missing. i am trying out hole milling option.

3 REPLIES

Re: Not get I J and K values.

Phenom
Phenom

Check I J And K word values are not modal

 

PB_Word_modal.PNG

Re: Not get I J and K values.

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

its the same as suggested....no changes....still no IJK output

Re: Not get I J and K values.

Gears Phenom Gears Phenom
Gears Phenom

Have you added the PB_CMD_init_helix custom command ?

 

From the custom commands click Import, it shoud default to the custom_commanf folder and select the pb_cmd_helix.tcl file.  This has instructions on where to place the command.  If this is not aded to the post you will not get helical output.

 

 

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Learn online





Solution Information