Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Nx12 adaptive milling

Valued Contributor
Valued Contributor

Is ther a way to change the cut levels to start at the deepest level then step up to the next intead of from the top down

(in one operation)

 

21 REPLIES 21

Re: Nx12 adaptive milling

Legend
Legend

When I have wanted to do this a few times... usually cavity milling an exterior surface...

 

Right click on the path, --> toolpath --> edit.... Hit the reverse button.

 

Will now cut from the bottom up.

It's a total reversal, so if you want to climb. the initial path will have to be conventional.

And if you regenerate the path it will go back to top down.

 

So, I usually lock the path (I have lock override off in the customer defaults)

If I want to regenerate the path, I will have to take the time to unlock it first.

Saves me from messing up good proven path.

 

Good Luck, Paul S.

{Paul Schneider}, {CNC Programmer}, {DRT-Rochester}


Production: {NX11.0.2,MP5, NX12.0.2, MP4}

Re: Nx12 adaptive milling

Valued Contributor
Valued Contributor

 

Should have thought of that ,actually use the ole double reverse for flow cut sometimes

Just thought I would get the ball rolling early on this one

 

 

Re: Nx12 adaptive milling

Valued Contributor
Valued Contributor

Don't think that way is going to work very well

can't find a wat to change it from cutting from outside toward  inside

when you reverse it it cuts from inside toward outside

Re: Nx12 adaptive milling

Valued Contributor
Valued Contributor

 

also would really have to be creative with engage and retracts

not good

 

Re: Nx12 adaptive milling

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

This is the initial phase to allow users to make sure the base function is working properly.

There will be additional functions added to it step-by-step.

VoluMill and iMachining have started with a simple tool path a decade or more ago, so expect to have the system evolve for some years.

In the past CAM operations have been added with all the bells and whistles, nothing worked, no user used it, no problems have been reported and so the operation was only improved by accident.

Now new CAM operations come with the bare minimum of functionality, which works in the majority of situations up to specified limitations. Additional features will be added in phases, so that the enhancement is less likely to destroy the existing functionality.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Nx12 adaptive milling

Valued Contributor
Valued Contributor

This is why I am asking these questions now

I realize that I am working with a beta version

Been through a lot of headaches in the 25 yrs Ive used this software

Got to keep pushing though

 

 

Re: Nx12 adaptive milling

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@robber80 wrote:
I realize that I am working with a beta version

This is a production release, but it is the initial phase.

Remember contour profile, starting out with the bare minimum for swarf milling, afterwards a tilt angle, support for more tools, the ring height, etc. were added, each in a separate phase.

If I remember correctly, in the final stage there will be at least 80% of the functionality offered that VoluMill and iMachining offer. I doubt that the separate feed manager will be a feature, since NX already offers similar functions in a different way.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Nx12 adaptive milling

Valued Contributor
Valued Contributor

My bad was refering to what comes up when I log onto 12 It says Its a beta version

O I remember lots of new things that didn't work and the old stuff that still didn't work

Not looking to bad mouth the software

But have been through the mud

Looking forward to the 80%

 

Re: Nx12 adaptive milling

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi all,

 

thank you for this question. Adaptive Milling is released in NX12 as a first basic version.

 

NX CAM development works Agile, so we are releasing smaller pieces of functionality which we think will give the user value. The customers don't have to wait years to get a complete functionality anymore. Adaptive Milling is a good example for this.

 

With that being said, we are already working on enhancements for Adaptive Milling. Upcoming new features will be the Bottom Up Cutting and a Custom Spindle Speed for Helical Engange Moves.

 

@robber80 This features should addres your request.

 

Cheers,

Alexander

Lead Product Manager - Mold & Die

Learn online





Solution Information