Cancel
Showing results for 
Search instead for 
Did you mean: 

OOTB probing for Heidenhain

Pioneer
Pioneer

Are there any OOTB  probing for Heidenhain.  TNC530.

 

 

3 REPLIES 3

Re: OOTB probing for Heidenhain

I also am trying to add Probing output to a iTNC 530 post using Post Builder. Is there any OOTB functionality for this, or should I just edit the Fanuc Probing default post?

Re: OOTB probing for Heidenhain

Pioneer
Pioneer

I am interested in this as well. We use almost exclusively heidenhain and it would be very nice if this were available.

 

Thanks

Owen Fredericks
Manufacturing Engineer

Re: OOTB probing for Heidenhain

Valued Contributor
Valued Contributor

I added probe cycles to the command list in the machine configurator which call a subprogram with the cycle number. This is not perfect, but good enough for me. The subprogram is just heidenhain code. So far I only add probe cycles with an UDE in NX. These will be written out as a HH probe cycle which will be simulated by the CSE controller.

 

For very specific coordinate measurements, CYCLE 427, I used handwritten nc code but simulated it in NX.

 

It is a work in progress, depending on what is needed I add features.

W10 NX12.0.2.9
testing v1847

Learn online





Solution Information