Cancel
Showing results for 
Search instead for 
Did you mean: 

OUTPUT CSLF FILE NAME TO NC PROGRAM NAME

Pioneer
Pioneer

Hello again,

What a great forum.

 

I would like to find a setting if it exist to change the CSLF out file name to that of the NC PROGRAM name I want to output.2017-10-28_10-55-29.png

Currently it always outputs the NX File name as default until I change it.

 

I have several programs in the same NX file. I highlight the program to output and want to have that program name as the file name I output. Already there.

 

4 REPLIES

Re: OUTPUT CSLF FILE NAME TO NC PROGRAM NAME

Legend
Legend

Hi,

Directly you can't ,It depends on what you have select on the ont.

I know this solution:

Tcl :

Rename your program at the end :

file rename ...

Help tcl : File tcl tk

I'am not familiar , but a journal (Vb,C#,...) may be a solution :

Some help (vb) :

-Select your program  , look this way : ugopen\Sample....\vb.net\...OntSelection.vb

  -Select directory : system.windows.forms.folderbrowserdialog

    -run :Outputclsf 

Take a look at this topic :

Post-Processing-each-group-of-programs-to-separate-file

Production: NX11.0.2.7,VERICUT 8.1.2
Development: Tcl/Tk, Gnuplot
www.adgroupe.com

Re: OUTPUT CSLF FILE NAME TO NC PROGRAM NAME

Gears Legend Gears Legend
Gears Legend

Here's a vb journal that does just that.

You can select multiple groups, to get multiple CLS file's

They are stored in the workpart folder in a sub folder CLS

 

Patrick Delisse
KMWE - Aero Engine
NX 12.0, TC 11.2, CAMPOST V22, Vericut 8.2, TDM 4.8
C#, VB, .NET

Re: OUTPUT CSLF FILE NAME TO NC PROGRAM NAME

You might also read about library output - it's a keyword in the configuration .dat file. 

Mark Rief
Retired Siemens

Re: OUTPUT CSLF FILE NAME TO NC PROGRAM NAME

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Probably the easiest thing for you is to use the journal option.

 

As the CLS output is done thru tcl & def files that are *similar* to the equivalent post files (just without the PUI) you could also copy one of the existing definitions & manually edit the tcl (use MOM_start_of_group / MOM_end_of_group, IIRC)

 

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information