Cancel
Showing results for 
Search instead for 
Did you mean: 

Object - Customize from

Genius
Genius

Is there a file similar to cam_gerenal.opt, that you can add to, so that the Object - Customize From dialog box has more choices in the Objects In list? I have setup the library_dialogs file to have all my custom operation templates and would like to add it to that list so I don't have to browse for it every time that NX is restarted.

Mike Diamond, CNC Programmer, Orizon Aerostructures Inc.

Production: NX10.0.3.5, Vericut 8.1.4, ICAM V21
Development: VB.NET, Tcl/Tk
Testing: NX12
2 REPLIES 2

Re: Object - Customize from

It only shows the parts open in your session.

If you open library_dialogs first, and then open your part and use customize_from, does that help?

Mark Rief
Retired Siemens

Re: Object - Customize from

Genius
Genius

Yes. I can handle that as a workaround.

 

Thanks Mark

Mike Diamond, CNC Programmer, Orizon Aerostructures Inc.

Production: NX10.0.3.5, Vericut 8.1.4, ICAM V21
Development: VB.NET, Tcl/Tk
Testing: NX12

Learn online





Solution Information