Cancel
Showing results for 
Search instead for 
Did you mean: 

Object Transform?

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi,

 

I recently updated NX 12 to the 12.0.2.9 and I noticed that the Object Transform is no longer available on the right click over an operation. 

 

I found it on Menu-Tools-Operation Navigator-Object-Transform but I cannot use it,

 

transform.png

 

How can I use it?

 

thanks! 

 

7 REPLIES 7

Re: Object Transform?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

hi

what you are showing is not right click on the operation

I have NX12.0.2.9 and transform is working

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Object Transform?

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

transform1.png

 

There it is with right click over the operation.

Re: Object Transform?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

adc.jpg

 

Strange.....

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Object Transform?

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

what MP do you have installed?

 

here's mine 

 

transform2.PNG

Re: Object Transform?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

patch - none, so could be difference

If you have problem, report it to GTAC

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Object Transform?

Siemens Phenom Siemens Phenom
Siemens Phenom

Was some kind of editing performed to the tool path? That may be preventing you from seeing the Transform function. For example, if I use Divide by Holder on a Cavity Mill operation I do not see the Transform function afterward. Another example is if I use Mirror on the operation. Neither the mirrored op nor the original op can have a transformation performed on them.

Re: Object Transform?

Legend
Legend

I have a network install... went from 11 to 12, tried to cheat and run in the network enviroment with the NX11 mach files. Lots of things missing or squirrley

 

Set it up right all the options were there. Install issue

{Paul Schneider}, {CNC Programmer}, {DRT-Rochester}


Production: {NX11.0.2,MP5, NX12.0.2, MP4}

Learn online





Solution Information