Cancel
Showing results for 
Search instead for 
Did you mean: 

Okuma CSE drilling cycles

Valued Contributor
Valued Contributor

Hello

 

Im making a okuma based machine and I was wondering no drilling cycles was included with of the box examples.

Does okuma cse driver use cycles, should i copy them from fanuc model?

 

 

4 REPLIES 4

Re: Okuma CSE drilling cycles

Legend
Legend
Normally no cycles are included in the OOTB.
You can get the cycles from the machine vendor, and then insert it to cse_driver/subprog.

regards

Re: Okuma CSE drilling cycles

Valued Contributor
Valued Contributor

Thanks I'll contact Okuma then.

 

Re: Okuma CSE drilling cycles

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello!

@jussi, when I build MULTUS B300, it was a same problem for me. Just for quick solution I create my VERY SIMPLE subprogramm, for example - for 181 cycle:

 

O181 (Drilling)

G1 Z[VZDEP] F423
G1 Z[VZCUR] F423

 

JUST FOR SIMULATION! Of course, you can create more complex and detailed cycles. You can try use cycles from real CNC - but.....

 

Re: Okuma CSE drilling cycles

Valued Contributor
Valued Contributor

Hello Yuri

 

Thank for "quick and dirty" solution, this is what I was looking for.

Im only doing exhibition demos, so these do not need to be exact machine cycles.

 

I was thinking this cycle thing too complicated... and just looking a real cycles.

 

Learn online





Solution Information