Cancel
Showing results for 
Search instead for 
Did you mean: 

Omit code using Linked post

Valued Contributor
Valued Contributor

Hello.
I have 5x post processor, Master (Mill) with 2 linked(HEAD) posts (RAH)+(PROBE)

Probing post is empty...used to output logic written in Mill Control...

In Master post,  there 2 cc at tool change and at end of program giving me grief...

Using code below overcomes the issue when in PROBE mode...but when in Mill & RAH mode, 2 cc don't excuted anymore...

# kal added  3-9-18

  global mom_sys_postname
  
  if { ![info exists mom_sys_postname(PROBE)] } {
    
  cc logic to omit ...
        
   } 
  
  # kal added  3-9-18

 
Thanks in advance for your help.
 Kal.

NX 9.0.3.4 MP12 | PB 9.0.3.2 | NX11.0.2.7 MP12 | VERICUT 7.3.4
1 REPLY

Re: Omit code using Linked post

Gears Phenom Gears Phenom
Gears Phenom

Where is this custom command located at start of program, at tool change ?

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Learn online





Solution Information