Cancel
Showing results for 
Search instead for 
Did you mean: 

Operation using curves

Builder
Builder

Good day,

 

Is there any way to select multiple curves at once when using planar mill or 3D profile.

When I select multiple curves at once they automatically connect each other.

The only way I can do now is to select the curves one by one to separated them when generating tool path.

 

Thank you always.

Jayson

 

2 REPLIES 2

Re: Operation using curves

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes, there are a few different ways of selecting multiple curves as boundaries depending on what you want to do.

 

First, when the Boundaries Selection Method is set to Curves, look into the different Curve Rules in the Top Border Bar.

Capture32.JPG

The Tangent Curves and Connected Curves options are usually popular choices.

 

However, users don't always want to select an entire chain of curves that are tangent or connected. There is another method to select the beginning and end of a chain and automatically get all the curves in between.

 

To do this you must first have your Selection Method set to Curves as before. Next, select the More icon next to the Curve Rule menu, which looks like a little arrow.

Capture34.jpg

When the Options dialog opens, check the Chain Between box and select Close.

Capture35.JPG

Upon exiting the Options dialog you will notice that the Curve Rule has automatically been set to Connected. Now you can select just two curves along a chain and NX will fill in all the rest between. The key is to select the curves at at the ends pointing toward each other.

Capture36.JPG

Now the curves in between will also be selected.

Re: Operation using curves

Builder
Builder

Hello jkane1,

 

Thank you for your response.

I am sorry my question is not clear, this is not what I am looking for,

what I want is to select non-connected multiple curves from 3D profile or planar mill operation

using open curves option. When I select a non-connected multiple curves it automatically connect all the curves.

Is there no option that I can select all the non-connected curves then automatically populate all the curves under the list of curves dialog box. Now I select non-connected curves by clicking the add new set button, but mostly I have hundres of curves to select. I am also aware of the fixed contour operation with curve/point drive method, there I can select multiple non-connected curves at once but I cannot make extended tool path.

MultipleCurvesSelection.JPG3D Profile Opertion

Thank you Always,

Jayson

Learn online





Solution Information