Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Optimize Feed rate while generating

Creator
Creator

Hi,

 

How Optimize Feed rate while generating option works ?

How to use Optimize Feed rate while generating for Planar Mill ?

 

regards,

ADP

4 REPLIES 4

Re: Optimize Feed rate while generating

This does exactly the same thing as the command in the Operation Navigator - RMB > Tool Path > Optimize Feed Rates. If you have a path that takes a long time to generate, and you want to try several itterations of optimize, then the command in the Operation Navigator is the easiest. If you know your optimization parameters up front, you can enter them in the feeds and speeds dialog inthe operation, and the optimization is done automatically after the path generates, so that you don't need to remember if you regenerate later.

Mark Rief
Retired Siemens

Re: Optimize Feed rate while generating

Pioneer
Pioneer

Hi

 

Witch file (tcl) controls this optimization process. Does CAM user has ability to modify rules of optimization?

 

marek

Re: Optimize Feed rate while generating

Legend
Legend

I belive this is at the CLSF level. It is not part of the post as far as I know. 

Glenn Balon
Production: NX 12.0.2 MP7 Primarily CAM

Re: Optimize Feed rate while generating

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I believe this is part of the internal toolpath generation (inside NX DLLs, assuming you select the correct options inside the dialogs)

The CLSF and post output just reflect what is already optimized.

 

 

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information