Cancel
Showing results for 
Search instead for 
Did you mean: 

Optimized to Drive for Tool Axis

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Dear All,

I can't use Option Optimized to Drive for Tool Axis , and away have an error the same picture. Who can help me to know or give me an example for Optimized to Drive .

1.png

5 REPLIES 5

Re: Optimized to Drive for Tool Axis

Solution Partner Genius Solution Partner Genius
Solution Partner Genius
You must set any maximum lead angle (Angle parameter). If there is 0 set, tool cannot have any lead Angle - but you want have some lead angle to have Heel Clearance 0.02. So you must allow tool to have some lead. Try to set to Angle parameter some value (between 2 and 88 as error message says).
Vavrusa Ondrej
NX10.0.3
NX11.0.x testing

Re: Optimized to Drive for Tool Axis

Attached in an old sample that shows optimized to drive - also known as curvature matching. You can check out the parameters in these operations.

Mark Rief
Retired Siemens

Re: Optimized to Drive for Tool Axis

Legend
Legend
Hi Mark, Please see attached image for the message I am getting when I try to regenerate the path in the file you have shared. What's the meanig of this? DO I need any additional license or any setting to be done?

Re: Optimized to Drive for Tool Axis

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Mak_Jo wrote:
DO I need any additional license or any setting to be done?

Yes, optimize to drive is a separate license.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Optimized to Drive for Tool Axis

If you talk to your reseller or account manager, the add-on is called Curvature Matching [NX30407]. 

This activates the additional option for Tool Axis called “Optimized to Drive”.

Mark Rief
Retired Siemens

Learn online





Solution Information