Cancel
Showing results for 
Search instead for 
Did you mean: 

Organize the CAM Process

Pioneer
Pioneer

01. You put the Stock on Wise

02. Machine the Part (TOP Machining)

03. Put the part 180 deg in Wise for Bottom Machining

 

How many files you have for a Manufacturing Part ?

I mean, do you have one file for TOP machining and another for Bottom Machining

What is the best way to organize the process ?

14 REPLIES

Re: Organize the CAM Process

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The best way is to have each setup in its own part file. This makes it much easier to do machine simulation of each situation.

If I remember correctly the machining line planer, included since NX 10 at least, should simplify the process of creating multiple setups. There is a video by @TomvantErve in the community.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Organize the CAM Process

Siemens Phenom Siemens Phenom
Siemens Phenom

We do recommend that users make a new file for every machine setup they create. This has a few advantages.

  1. File managment. Other users opening your file will always know what side is being machined for the single setup.
  2. Smaller file sizes. Each setup file has only the operations and tool path data for that file. This means better perfomance.
  3. Design protection. A proper manufaturing setup file brings the designed part file in as an assembly. This means that the CAM programmer cannot modify the original part while creating tool paths. He can create a copy of the geometry so that he can modify it for optimal tool path creation, but the original design intent is protected.

On the other hand, all setups and tool path data can be made in just one file. Mutiple MCS objects can be made for each setup on the part. The operations under each MCS in the Geometry View will be oriented to their parent MCS. This has the obvious advantage of having to manage only one NX part file rather than several files together.

 

The choice is up to you. Siemens has what we consider to be best practices, but your workflow should dictate what is right for your shop.

Re: Organize the CAM Process

Pioneer
Pioneer

Thanks all. I am in practice mode ! I am doing this :

- Create TOP file asm : add Part - add wise/clamps - link body all

- Create operation for TOP machining

Now I have a problem.

- When create Bottom file, I want the IPW from Top and I can not bring it to file (NX 11)

- But if I create parasolid of IPW (which I do not want), I have another problem since wise setup from Top it is not good for Bottom !!!

Also, is anywere a Setup in NX to put a clearacnce to "Specify Check". I see the Tool is JUST avoiding it but I would like to put like 1mm clearance to it.

Re: Organize the CAM Process

Pioneer
Pioneer

Hmmm, I have Manufacturing but I do not have File - New - Manufacturing option ! 

This is maybe the reason for IPW

 

Re: Organize the CAM Process

Siemens Phenom Siemens Phenom
Siemens Phenom

Edit the Workpiece object in the second setup file. Select the same part geometry as before. Now in the Blank Geometry definition, select the pull-down menu at the top and select IPW - In Process Workpiece.

Capture3.JPG

 

Now select the Select Source for IPW button and browse for your first setup file. Select the Workpiece object from that file and select OK. Select the Update Local IPW from Source button and you should see a facet model in the graphics. Select OK and the roughing operations will use this to calculate IPW regions.

 

Let us know if this works.

Re: Organize the CAM Process

Pioneer
Pioneer

"The part containing the source for IPW must reference the same component for Part geometry as the work part"

Highlighted

Re: Organize the CAM Process

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

That is not a problem:

First setup:

CAM-Part-Machine-Top
    |
    +- CAD-Part

Second setup:

CAM-Part-Machine-Bottom
    |
    +- CAD-Part

You always have the same CAD-part file as the component in each CAM setup part. The fixture, machine, etc. can be different, only the design part must be the same.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Organize the CAM Process

Pioneer
Pioneer

Got it, thanks a lot...

Re: Organize the CAM Process

Genius
Genius
Dear jkane1,

I hope one day Siemens wakes up an notices their recommendation is against FBMs principle to do generate all machining operations in a single CAM part.
Best wishes,
Joachim

In production NX 12.0.1.7 D2
In testing NX 12.0.1.7 MP4

Learn online





Solution Information