Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Outputting the cdc d value

Valued Contributor
Valued Contributor

I would like to post the value of the D number from the cdc in the operation header.Would i output Literal Address D=? I couldnt find the mom varaiable for this.

31 REPLIES 31

Re: Outputting the cdc d value

Valued Contributor
Valued Contributor

CDC.PNG

Re: Outputting the cdc d value

Valued Contributor
Valued Contributor

The (CDC=D04) is what im looking for

Re: Outputting the cdc d value

Gears Phenom Gears Phenom
Gears Phenom

I dont know what CDC is. Doesnt matter.

What variable do you want to find? For the D or for its value?

How do you search variables?

But if you get the output of D by default - it exists ofcourse.

What about looking into D address or do debugging.

Anyway, if variable doesnt exist in the moment when you want - it doesnt exist. end.

 

if you want CDC=D instead of D  just rewrite the D to CDC=D etc..

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Outputting the cdc d value

Valued Contributor
Valued Contributor

I ran the debug and the line for the d number reads Address D=04 cdc is the cutter compensation the D represents the offset being used

Re: Outputting the cdc d value

Gears Phenom Gears Phenom
Gears Phenom

1. so adjust it in postprocessor, rewrite D to CDC=D in D address/word.

 

2.debugging  I mean to find variable - debugging creates  3 extra files with variables, MOMs etc.

Where you can find variable with value 04.

Also you can see it in D address expression.

And then you can use it in new address or output literal with format.

 

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Outputting the cdc d value

Valued Contributor
Valued Contributor

Im still  new to tcl when I ran the debug and selected the line that the D number outputted on it read Address D=04. I didnt see a mom variable unless im doing it wrong I looked at the variable list and did see mom_cutcom_adjust_register was thinking this might be the variable but not sure.I tried an output literal for this too see what would post but nothing posted out.Sorry if I dont follow what your saying like i said its new to me Im going to take a class but the next one in my area isnt till March

Re: Outputting the cdc d value

Gears Phenom Gears Phenom
Gears Phenom

D address with variable mom_cutcom_adjust_register is outputed or exists only when you have cutcom turned ON in the operation.

 

Also you have to turn on this check blocks:

Snímka.JPG

Then you will get :

N0030 T02 M06
N0040 G00 G90 X-74.559 Y57.918 S650 M03
N0050 G43 Z86. H05
N0060 Z68.
N0070 G01 Z65. F250. M08
N0080 G41 X-90. Y55.417 D06
N0090 Y40.417
N0100 Y37.417

 

*Notice that D address is modal and also optional in the block (means if doesnt exists doesnt give error)

Bez názvu.jpg

 

*Notice I have D in rapid move too and as you see above there is no D - because in that moment variable doesnt exist.

 

If you want make CDC=D from D - just rewrite it - edit address:

Snímkd.JPG

BUT if you want to have it on the beginning of the program - it is immposible with this variable- it doesnt exist so soon.

 

You have to find other variable which carries value you entered in the tool and exists sooner.

If you were browse the debug files - 3 text files, you can find for example : mom_tool_cutcom_register

And it represents number entered in the tool as cutcom register.

Or if your cutcom numer can amtch with the tool number- you can use it.

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Outputting the cdc d value

Valued Contributor
Valued Contributor

Just want it to out put literal at the operation header so the operator knows the tool is using the cdc and what number it is

Re: Outputting the cdc d value

Valued Contributor
Valued Contributor

(**********************************)
(  TOOL NUMBER   4  )
( THREAD_MILLING )
( TOOL:10_32_THREADMILL )
( DIAMETER:0.120 )
( TOOL NOSE RADIUS:0.000 )
(CDC=D04)
(**********************************)

This the output header im currently posting but i edit in the (cdc=d04) line i wouls like it to output this automatically

Learn online





Solution Information