Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Overview of which Tool work with which Operation?

Pioneer
Pioneer

Hello,

Example i like to chamfer a part.  I take a chamfer with tracking point and the planar pofile operation. The same operation doesn't work with a "user_defined tool" with a tracking point. So where i can see what Tool works with whar operation?

 

NC Programmer
NX 11.0.1.11
1 REPLY

Re: Overview of which Tool work with which Operation?

Gears Phenom Gears Phenom
Gears Phenom

user defined tool can be used only wth planar profile operation

https://docs.plm.automation.siemens.com/tdoc/nx/12.0.2/nx_help/#uid:xid1128418:index_mfgmilling:comm...Smiley Tongue

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Learn online





Solution Information