Cancel
Showing results for 
Search instead for 
Did you mean: 

PMI details not recognised in Feature Based machining

Creator
Creator

I have added PMI to a feature.Then Using Teach feature,added the feature in the library.

But I cannot see PMI details in Attributes.

Question is how to make PMI to appear in Attribute details?

 

Check the attached presentation.

 

NX version 9.0.3.4

 

thanks !!

 

 

 

 

3 REPLIES 3

Re: PMI details not recognised in Feature Based machining

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

Please have a look at this tech tip video.

You need to add a name to each of the PMI dimensions to tell FBM which dimensions you are interested in, what to call them and then the software will use the PMI geometry association to derive a recognition rule that will pickup both the actual dimension and the dimension tolerance.

 

So instead of the Ø50 ± 0.1 you need to use Ø50 ± 0.1 MY_DIAMETER.

This will tell FBM to add MY_DIAMETER, MY_DIAMETER_UPPER and MY_DIAMETER_LOWER attributes to your feature (shown in the dialog on your slide #4) and populate them with the proper values.

 

Best of luck,

 

Tom van 't Erve

NX CAM Development

 

Re: PMI details not recognised in Feature Based machining

Creator
Creator

Hi Tom,

 

thanks for the reply,Video is very helpful.

Its working fine except the below case .

 

I have created Lightweight section and applied PMI by picking up the arc and second by corner edge blend,also named it (see images below) .Only R5 RAD_1 shows up in attribute list but not R5 ARC_SEC.

 

What may be the reason.

 

 

1-FBM.jpg

 

 

 

regards,

 

 

 

Re: PMI details not recognised in Feature Based machining

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You can only use real geometry, since the attributes must be associated to an existing edge or face.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Learn online





Solution Information