Cancel
Showing results for 
Search instead for 
Did you mean: 

POST_BUILDER HELP

Creator
Creator

I need help edit files post

I need feed rate exactly as I specify

thanks!

 

2017-09-20_085618.jpg

3 REPLIES

Re: POST_BUILDER HELP

Gears Phenom Gears Phenom
Gears Phenom

You have to edit format.

To be sure the feed is 0.5 - just output literal feed value in motions and you can see that feed is 0.5....

But in block/address output it is F1.

So definitely it is by format setting.

 

Snímka.JPG

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: POST_BUILDER HELP

Creator
Creator

thank you !!!

Re: POST_BUILDER HELP

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

ALso (same dialog) make sure the "min" value for each appropriate feedrate type (xPM, xPR, DPM, etc.) is "small enough"  (for IPR I would set the min to .0001 or similar) 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information