Cancel
Showing results for 
Search instead for 
Did you mean: 

POST DEVELOPMENT FOR 4-AXIS FANUC CONTROL

Creator
Creator

Hello,

 

I am making post for 4-axis fanuc control. i create a VARIABLE_CONTOUR operation  and post processed.

but in output nc file A axis didn't come with feed. 

 

please help me out for this issue. or suggest me which CMD command is used for this output requrement.

 

3 REPLIES

Re: POST DEVELOPMENT FOR 4-AXIS FANUC CONTROL

Siemens Legend Siemens Legend
Siemens Legend

can you attach a small sample and the post

Re: POST DEVELOPMENT FOR 4-AXIS FANUC CONTROL

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Post Builder or Post Configurator?

 

guessing...

In Post builder..

Check "Program and tool path" tab -> "Program" tab -> Select "Machine control"

Scroll down & select "Feedrates" box

Scroll that dialog down.  For "Rotary Only" and "Linear and Rotary" feedrate modes, you probably want to set them to "DPM" (degrees per minute)

Most (if not all) Fanuc contrls treat the "F" word in any G1 motion with rotarymovement as "Degrees per minute"

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: POST DEVELOPMENT FOR 4-AXIS FANUC CONTROL

Creator
Creator

dear ken,

 

thanks,

 

now its working and output is ok.

 

just i want to know what feedrate we need to use for DPM or for A-axis?

 

by default it is 100. Is it feasible or need to use other one?

 

 

Learn online





Solution Information