Cancel
Showing results for 
Search instead for 
Did you mean: 

Parallel Created 3D IPW resolutions

Valued Contributor
Valued Contributor

Hi,

 

Is there a way to control the resolution of the 3D IPW thats created with "Parallel Create 3D"?

I'm working with a large part ø1200 x 200 and when I use "Parallel Create 3D" I get an polygon.

If I want an accurate 3D IPW I have so use "Verify Tool Path" and save that IPW.

 


Regards,
Sven

NX11.0.1
10 REPLIES 10

Re: Parallel Created 3D IPW resolutions

Siemens Phenom Siemens Phenom
Siemens Phenom

That action will use the IPW setting from "Medium".

You can change that in the customer defaults or in the CAM Preferences.

 

Hope that helps

 

CAM_pref_ipw_medium.jpg

 

CD_IPW_MEDIUM.jpg

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: Parallel Created 3D IPW resolutions

Valued Contributor
Valued Contributor

Hi Thomas,

 

Thanks for the response.

 

I dit some testing but the result was not what I was expecting.

When I use Parallel Creat 3D this looks nothing like the 3D IPW thats created with Verify toolpath on medium settings.

 

On the left you can find the one thats generated with Parallel Create 3D and on the right is the one from Verify Toop Path on medium settings

3D-IPW_Parallel-Create-3D.png3D-IPW_Verify-Tool-Path.png


Regards,
Sven

NX11.0.1

Re: Parallel Created 3D IPW resolutions

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Sven,

 

thanks for addressing this by some snapshots. I really like to give you some hints, but based on this information only it is hard to tell why these differences appear. Could you either describe in more detail what you are doing or - as it looks like a simple part - provide the description and part through GTAC, so that we can have a closer look to it?

 

Thanks

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: Parallel Created 3D IPW resolutions

Valued Contributor
Valued Contributor

I made this part just to show the difference between the 2 functions.

The part that I'm working on is a bit more complex but I cant share it on an open forum.

 

We have Siemens NX from a local reseller so we don't have direct support from GTAC?
I can't create an IR...

 

I can try to explane more what I'm doing but its really simple.

When I use Verify Tool Path, set the IPW settings to medium (same as Parallel Create 3D function as you said)
and save that IPW then I get a good 3D IPW (left picture). 

If I use Parallel Create 3D then it generates a 3D in the background but the result isn't the same. (Right Picture)


I like to generate the 3D IPW in the background so I can still work on the part. This is the intention of the function I think?


Regards,
Sven

NX11.0.1

Re: Parallel Created 3D IPW resolutions

Siemens Phenom Siemens Phenom
Siemens Phenom
Your assumption for what "Parallel Generate" should be used is correct.
I have another idea what could be the root cause, but need more time to check on my end.

I like to ask you to check what are your settings of:
* intol/outol of the operation
* the chordal tolerance in Manufacturing Preferences -> Geometry
Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: Parallel Created 3D IPW resolutions

Valued Contributor
Valued Contributor

Intol/Outtol is set to 0.005mm

 

And below you can find my settings for the tollerance.

image.png


Regards,
Sven

NX11.0.1

Re: Parallel Created 3D IPW resolutions

Siemens Phenom Siemens Phenom
Siemens Phenom

Ok thanks, I assume the result should be the same if these values are the same.

  • Verify is using the chordal tolerance.
  • Operation generate (as well as parallel generate) is using the operation settings intol/outtol
Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: Parallel Created 3D IPW resolutions

Valued Contributor
Valued Contributor

Ok, good to know..

But how do I get these 2 methods to produce an 3D IPW with roughly the same resolution?


Regards,
Sven

NX11.0.1

Re: Parallel Created 3D IPW resolutions

Siemens Phenom Siemens Phenom
Siemens Phenom

MAybe I was not precise.

If the intol and chordal tolerance are the same - as well as medium needed setting is used in both cases - also the created IPW should have the same resolution.

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Learn online





Solution Information