Cancel
Showing results for 
Search instead for 
Did you mean: 

Parameters Mazak, iso /fanuc

Gears Phenom Gears Phenom
Gears Phenom

hello,

Could somebody tell me what numbers of parameters is allowed to use for any purpose (not to overwrite some system parameters) and how to properly set it?

For example:

#50=123

 

Thank you for answers

j

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #
9 REPLIES 9

Re: Parameters Mazak, iso /fanuc

Pioneer
Pioneer

Macro programing elements in fanuc control units.It can be used system variables of fanuc units.

 

But I am begineer macro programing in fanuc controller. I do not want to wrong code but something like that.

 

#1=0
#2=20
N1G3X50Y0I-50F1000
Z-#1
#1=#1+1
IF[#1LE#2]GOTO1

Re: Parameters Mazak, iso /fanuc

Gears Phenom Gears Phenom
Gears Phenom
Thanks
because when I set #50=1 and use it in H#50 it returns some error in mazak.
---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Parameters Mazak, iso /fanuc

Pioneer
Pioneer

I have not seen usage of H#.You can manipulate macro codes in SWAN soft. It might be usefull.

 

And I will ask my friends where is this error coming.

Re: Parameters Mazak, iso /fanuc

Phenom
Phenom
#1-#33 are local variables that should be available. It is not usual to have #34-#99 available. #100-#199 and #500-#XXX are globals.
NX12.02
Windows 10 Pro
ITC Inc.

Re: Parameters Mazak, iso /fanuc

Gears Phenom Gears Phenom
Gears Phenom
Thanks I will test it
---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Parameters Mazak, iso /fanuc

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom
If your going to start using Macro B I would recommend
CNC Programming using Fanuc Custom Macro B by S.K Sinha

Good examples
John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: Parameters Mazak, iso /fanuc

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You really need to consult your machine documentation & options purchased to determine which # variables are available for a specific machine. 

Typically for Fanuc machines, the # variables available are listing in the programming documentation.

You could also go to the control and "page down" thru the variables to see what is available.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Parameters Mazak, iso /fanuc

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

Just from experience you should also check is any of the macro variables are reserved.  For example the Renishaw inspection plus probing software uses many of the #500 level variables.  On many controls there is a limit on available variables. 

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: Parameters Mazak, iso /fanuc

Gears Phenom Gears Phenom
Gears Phenom

Thanks everybody

I am not working with amcro prorgaming (if I udnerstand well)

I just want to use variables.

I used #150 and it was OK.

#50 was probably out of interval for free variables. @Study

It ws already in manual for mazak.

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Learn online





Solution Information