Cancel
Showing results for 
Search instead for 
Did you mean: 

Parasolid and names of the components

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello!

 

I have a queation about names of the components in a parasolid file. If a parasolid file is opened with File/Open command, the assembly structure is created. Each solid body is added to its own file/component. The name of the component is also the same as it is the name of the solid body. With only one small difference.

If the solid body was named 'Test', the component comming from a parasolid file will have name 'Test_id6_x_t'.

Is it possible to set the naming of the components so, that there would be no _id6_x_t? So, that the name of the component would be exactly the same as it was the name of the solid body.

 

Thanks.

1 REPLY 1

Re: Parasolid and names of the components

This was cross posted in the design forum, so to keep all the answers together, please reply Here.

 

 

Mark Rief
Retired Siemens

Learn online





Solution Information