Cancel
Showing results for 
Search instead for 
Did you mean: 

Parse error PB []

Gears Phenom Gears Phenom
Gears Phenom

Hello,

 

I want output "G110 [B] 2" in the nc code.

When I write  MOM_output_literal "G110 \[B\] 2" in Postbuilder it gives me parse error.

 

any idea to make it work?

 

thank you

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #
7 REPLIES

Re: Parse error PB []

Phenom
Phenom

The front bracket probably works the way you have it. The back one may require creating a variable to contain "\]" and use that instead.

NX12.02
Windows 10 Pro

Re: Parse error PB []

Gears Phenom Gears Phenom
Gears Phenom

global k
set k "\]"
MOM_output_literal "G110 \[B$k 2"

it doesnt work too.

Now, I am looking for any solution to output : G110 [B] 2

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Parse error PB []

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Which version of Post Builder?
I just tried: MOM_output_literal "G110 \[B\] 2"

in PB 11, and it works OK

Marek Pawlus, NCmatic

Development: C#, Tcl/Tk, CSE

Re: Parse error PB []

Gears Phenom Gears Phenom
Gears Phenom

I have to apologise.

 

 MOM_output_literal "G110 \[B\] 2" works.

 

Parse error was in another line.

thank you.

later I will delete this thread.

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Parse error PB []

Phenom
Phenom

My comment was for if you are trying to get it through a block template def in the def file. MOM_output_literal has less constraints.

NX12.02
Windows 10 Pro

Re: Parse error PB []

Legend
Legend

the second "backslash" can be ignored...

\[B]

works too

Production: NX11.0.2.7,VERICUT 8.1.2
Development: Tcl/Tk, Gnuplot
www.adgroupe.com

Re: Parse error PB []

Phenom
Phenom

Nice - I will have to note that.

NX12.02
Windows 10 Pro

Learn online





Solution Information