Cancel
Showing results for 
Search instead for 
Did you mean: 

Part-Families with cam setup

Creator
Creator

Hi,

 

I have a project with many different Frames with features and so on...

I created my variant with a part familie!

 

Know i will make my cam-operations. In the "Master-Part" I will create all possible operations.

When I manage the part-family I can deactivate features...

Is it possible to manage the cam-operations by the same way. 

 

I have the problem that I can't save a family-member when I generate the toolpath and delete operations!

 

Is there a way how I can handle this?

 

Thanks for your feedback!!

 

2 REPLIES 2

Re: Part-Families with cam setup

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

No.

The best way to handle that is to use the family master as a component of a CAM setup part, using a linked body of the CAD design as the geometry for CAM.

To program the family childes, you would use save as on the CAM setup part and replace the component with the family child in question.

Since the child bodies share the same internal object IDs, faces and edges should be matched automatically when you update the linked body.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Part-Families with cam setup

Creator
Creator
Thank you Stefan,
this is the way I did it konw!

Learn online





Solution Information