Cancel
Showing results for 
Search instead for 
Did you mean: 

Plunge feed.

Pioneer
Pioneer
What is the best way to plunge at a certain feed rate? I noticed that there is not an actual setting for this. What I am trying to do is.... Rapid to .100 above the feature, feed into a pre drilled hole at a fast feedrate, engage into my cut at a slow feedrate (engage feed), and then cut at my cut feed rate.
NX 12.0.0 PB 12.0.0
13 REPLIES

Re: Plunge feed.

Genius
Genius

Hello,

 

You can define different feeds for different sections of you toolpath under the feeds and speeds section don't know if you have tried this?

Feeds and Speeds.JPG

 

Sorry if you have already tried this or you are looking for something else.

Regards

Dave
NX10.0.3MP13
NX11.0.1
Production
TC10
Vericut 7.3,7.4.1,8.0.2

Re: Plunge feed.

Pioneer
Pioneer

Dave,

 

I have tried these settings but haven't found a combination that gives me what I'm looking for. Doesn't mean it's not there, just haven't figured it out yet.

 

Thanks!

NX 12.0.0 PB 12.0.0

Re: Plunge feed.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Have you tried setting the approach feed to cut instead of rapid?

Have a look at the feeds and speeds dialog box and the non cutting moves dialog box for when which feed rate is used Smiley Wink

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Plunge feed.

Pioneer
Pioneer

I had tried that but now instead of Rapiding from a Z of 1.5 down to .1 and then feeding into the hole. It wants to feed from my initial Z of 1.5 all of the way down into the hole. I had checked into the help pages like you suggested but I was trying to get away from using start points to give me this result because I was hoping I could just specify something such as a Rapid Plane and a Clearance plane to control this.

NX 12.0.0 PB 12.0.0

Re: Plunge feed.

PLM World Member Creator PLM World Member Creator
PLM World Member Creator

Not sure what your toolpaths look like, but you should be able to control this with your non-cutting moves.  Most non-cutting moves have a height field that control your "rapid to" position as you see in the image.  If this isn't working then I suspect you should take a close look at your post in terms of how it outputs feedrates.

 

 

Re: Plunge feed.

Gears Phenom Gears Phenom
Gears Phenom

Since the "Height" is part of the engage move it will use the engage feed rate.  Without some customization to your post I don't see a way around this, without using the dreaded “start points” Even then you may not get exactly what you need.

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: Plunge feed.

You might look at the new Deep Hole Drilling operation introduced in NX 10.0.2.

 

It has more control of the spindle and feeds when entering a hole, like you use in gun drilling.

Mark Rief
Retired Siemens

Re: Plunge feed.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I was assuming this was for milling...

 

I would try setting a clearance plane, then possibly the approach feedrate would work.

Or use a Start point

 

Above should be reasonably associative

You can also use a "User defined event" "Goto" point with a specific feed, but they tend to have associativity issues (I think).

 

Another option is to redefine the horizontal clearance (where the yellow engage ends and where the cyan cut starts).  then engage could be the "faster" feedrate, but you drop down to the cut feedrate before reaching the part material.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Plunge feed.

Pioneer
Pioneer

Thanks for all of the replies. Here is the toolpath I am working with.

Capture2.PNG

It's a very basic toolpath (Planar_Profile) that uses a pre drill point to start on center and then back chamfers the hole with a Harvey Tool - Double Angle Cutter. For now I am just going to edit the vertical yellow line and override the feedrate, then when I get more time I will explore some other options.

NX 12.0.0 PB 12.0.0

Learn online





Solution Information