Cancel
Showing results for 
Search instead for 
Did you mean: 

Post Build: What should I put in my Post to generate a correct G code that performs holes? radius R

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Ok well first:

 

I am creating a Post Processor in post builder, generating a strategy (hole making) and testing on a 5 axis machine.

I'm not sure if I should adjust any option in the post for this case (5 axes).
The corresponding line comes out of the form:

G17 G03 X-35 Y-43 R.131

And well, I do not know if I'm missing something in the post or in the strategy (hole making)

I just got a mistake, although I have skipped several different, I have not been able to make the machine drill holes.

CNC ALARM 14040


Tried to change P.C. Upon linked GAP instructions

Sorry, we do not know the model or brand of the controller.

It is likely that if someone wants to help me you will need more information, ask and it will be given to you.

 

 

8 REPLIES

Re: Post Build: What should I put in my Post to generate a correct G code that performs holes? radiu

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
I can advise you:
1. Your cnc not supported R, may be. Try to use incremental or abs I and J.
2. Make short example manually, square 100x100 with radius at corners 10mm, more easy to understand problem.
3. If your CNC is 5 axis, how you switch ON RTCP? Sometime rtcp incompatible with G02.G03.

Re: Post Build: What should I put in my Post to generate a correct G code that performs holes? radiu

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Thanks Chigishev

Well, our cnc does support "R". We have checked it.

Can you tell me what is RTCP?

Re: Post Build: What should I put in my Post to generate a correct G code that performs holes? radiu

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

You wrote that your CNC is 5axis CNC. To control tool tip point "smart" CNC use a special function, RTCP or Rotary Tool Control Point - TRAORI for SIEMENS, G43.4 for FANUC or MAZAK, M128 for heidenhain.

 

Re: Post Build: What should I put in my Post to generate a correct G code that performs holes? radiu

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
I open SIEMENS 828 manual
Error 14040 - if you use circle Radius programming - it mean that start and end point idetiacal.

In Post Builber set output Quadrant Circles, not Full Circle.

Will be work.

Re: Post Build: What should I put in my Post to generate a correct G code that performs holes? radiu

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

@GonzalezD wrote:

Ok well first:

 

I am creating a Post Processor in post builder, generating a strategy (hole making) and testing on a 5 axis machine.

I'm not sure if I should adjust any option in the post for this case (5 axes).
The corresponding line comes out of the form:

G17 G03 X-35 Y-43 R.131

And well, I do not know if I'm missing something in the post or in the strategy (hole making)

I just got a mistake, although I have skipped several different, I have not been able to make the machine drill holes.

CNC ALARM 14040


Tried to change P.C. Upon linked GAP instructions

Sorry, we do not know the model or brand of the controller.

It is likely that if someone wants to help me you will need more information, ask and it will be given to you.

 

 

This ma be an obvious question but what are you trying to acomlish?

 

the code you referenced "G17 G03 X-35 Y-43 R.131" is for a circular move.  Are you trying to drill holes?

 

Without knowing what the control is you are just guessing on what the machine needs.  You must have knowledge of the machine requirements befor creating a post.


 

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: Post Build: What should I put in my Post to generate a correct G code that performs holes? radiu

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi,

 

Not Drill, im trying hole milling (throug) .26in

 

I think I'm doing the strategy the right way but ...
  Attached image.

Re: Post Build: What should I put in my Post to generate a correct G code that performs holes? radiu

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Thanks, I followed your advice to put in "circular record" "quadrant". One question, what should I put in IJK Definition?
-Vector - ArcStart to Center
-Vector - Arc Center to Start
-Unsigned Vector - Arc Start to Center
-Vector - Absolute Arc Center

Do you think that in this way, the strategy is starting where it ends?

I see that points 1 and 3, and 2 and 4 in each sequence are the same.
Besides X in N150 and N190 is the same.

I see everything well, what do you think?

Thank you

N0110 G00 X-35.9303 Y-43.7981 C0.0 B0.0 S2000 M03
N0120 Z2.2756
N0130 Z1.7472
N0150 G17 G02 X-35.9303 Y-43.7326 R.065
N0160 X-35.8648 Y-43.7981
N0170 X-35.9303 Y-43.8636
N0180 X-35.9957 Y-43.7981
N0190 G01 X-35.9303
N0200 G00 Z1.6578
N0210 G01 X-35.9957
N0220 G02 X-35.9303 Y-43.7326
N0230 X-35.8648 Y-43.7981
N0240 X-35.9303 Y-43.8636
N0250 X-35.9957 Y-43.7981
N0260 G01 X-35.9303
N0270 G00 Z1.7472
N0280 G01 X-36.0612
N0290 G02 X-35.9303 Y-43.6672 R.131
N0300 X-35.7994 Y-43.7981
N0310 X-35.9303 Y-43929
N0320 X-36.0612 Y-43.7981
N0330 G01 X-35.9303
N0340 G00 Z1.6578
N0350 G01 X-36.0612
N0360 G02 X-35.9303 Y-43.6672
N0370 X-35.7994 Y-43.7981
N0380 X-35.9303 Y-43929
N0390 X-36.0612 Y-43.7981
N0400 G01 X-35.9303
N0410 G00 Z2.2756
N0420 Y-30.8519
N0430 Z1.7472
N0440 G01 X-35.8648

Re: Post Build: What should I put in my Post to generate a correct G code that performs holes? radiu

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

If you use R - you no need any IJK values.

Learn online





Solution Information