Cancel
Showing results for 
Search instead for 
Did you mean: 

Post Builder 11.0.2 .1 Error

Valued Contributor
Valued Contributor

Keep geeting the following error:

 

Error: can't read "mom_sys_arr(Word_Seperator)": no such element in array

followed by

Error: window name "b" already exists in parent

 

when I select:

 

1) N/C Data Definitions

2) Other Data Elements

 

in Windows 10 Pro

 

Happens in existing post, sample posts and new posts??

 

Is there an easy way to downgrade Post Builder to an earlier release (to test for problem) or do I have to completely remove the software and re-install from scratch?

5 REPLIES

Re: Post Builder 11.0.2 .1 Error

Gears Phenom Gears Phenom
Gears Phenom

I get the same error.

Try to get into other data elements this way:

-program and tool paths - word summary - other data elements

 

Ive noticed another error:

Try to create lathe post, generic controler.

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Post Builder 11.0.2 .1 Error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

No way to "downgrade" other than un-install & re-install.

What I do is, when first installing a new version of NX:

- Install base version (e.g. NX10.0)

- Copy the install folder (e.g. copy "C:\Program Files\Siemens\NX 10.0" to "C:\Program Files\Siemens\NX 10.0_Base")

- then install MRs/MPs.

 

That way, if I ever need to "downgrade" I can...

1) RENAME the current version folder somewhere else (e.g. copy "C:\Program Files\Siemens\NX 10.0" to "C:\Program Files\Siemens\NX 10.0.3.5 MP16"

2) *COPY* (so you alway keep a "base" install) the "Base" folder to the install tree (e.g. copy "C:\Program Files\Siemens\NX 10.0_Base" to "C:\Program Files\Siemens\NX 10.0")

3) If needed, apply MRs/MPs as desired.

 

Note for Post builder, you can copy the entire post builder folder tree ("%UGII_BASE_DIR%\Postbuild") from one of the above folder trees to another, and rename it (e.g. copy C:\Program Files\Siemens\NX 10.0.3.5 MP16\Postbuild" to "C:\Program Files\Siemens\NX 10.0\Postbuild_1035MP16") .  Edit the "post_builder.bat" in that file, change the definition of "PB_HOME" as needed.  e.g.

set PB_HOME=%base_dir%\POSTBUILD_1035MP16

This way you can run a different version of PB than the rest of NX.

 

 

Ken "I have 9 different version of PostBuilder available for NX 10!" Akerboom

(edited to fix typos)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Post Builder 11.0.2 .1 Error

Valued Contributor
Valued Contributor
Hi Juraj and Ken_A,

Thank you very much for your replies!

Re: Post Builder 11.0.2 .1 Error

Gears Phenom Gears Phenom
Gears Phenom

anyway, repost issues to GTAC

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Post Builder 11.0.2 .1 Error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

See the solution center as it seems to be a known error.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Learn online





Solution Information