Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

[Post Builder] Block output range setting

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

Hi

 

I want to set it in Post Builder and output it like this:

 

ex)

request.jpg

 

 

How can I output to multiple blocks?

Please give me advice. Thank

1 REPLY 1

Re: [Post Builder] Block output range setting

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

What are you trying to do?

Have a maximum move length?

Note in surface contouring (possibly other operation types) there is a "MAX CUT STEP" that you could set to "1" to output individual moves.

 

If this is "3+2" machining (i.e. planar mill or floor/wall), why do you want MORE output?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information