Cancel
Showing results for 
Search instead for 
Did you mean: 

[Post Builder] Caxis rotation output setting

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

Hi

I am setting 5-axis machine of AC TYPE. I refer to sim08_mill_5ax.

 

My question is :

 

I want to output a value that rotates on the C axis as shown in the second figure.

If the current A axis is rotated a little bit, it is output to the C axis
Even if A axis is 0, we want to output to C axis.
Where do I set it up?

 

11.jpg

 

2 REPLIES 2

Re: [Post Builder] Caxis rotation output setting

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

User Def Event: "Lock Axis" should help. and set X or Y axis as locked.

Basically circle is the only shape you can make this way...

If you want to make for example a rectangle, it will require more calculations in postprocessor.

Marek Pawlus, NCmatic

Development: C#, Tcl/Tk, CSE

Re: [Post Builder] Caxis rotation output setting

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

Hi

 

I applied User Def Event: "Lock Axis" in front of me.

However, this has to be set by the user each time, The X and Y coordinates are output as fixed coordinates and thus are not correct.

 

Thank you for your advice.

Learn online





Solution Information