Cancel
Showing results for 
Search instead for 
Did you mean: 

[Post Builder] DATUM SHIFT

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

Hi

 

I have a related inquiry about DATUM SHIFT.

 

## Info

1. Version : NX11.0.2

2. Referance Machine : sim08_mill_5ax_tnc_mm

3. Controller : Heidenhain

4. Request : DATUM SHIFT value output

 

Open sample file. NX11\MACH\samples\nc_simulation_samples\sim08_mill_5ax_cam_tnc_mm.prt

 

The upper main mcs is set to the head side, and the local mcs is set to the lower side.

 

MAIN_MCS.jpg

 

Local_MCS.jpg

 

 

I try post processor.

datum_nc.jpg

 

I tried to change main mcs to the same location as local mcs.

 

MAIN_MCS_change.jpg

 

I tried the post processor again.

DATUM SHIFT Code block is not output.

I want the same settings as now. The post processor is currently configured via PostConfigurator.

(ref:MACH\resource\library\machine\installed_machines\sim08_mill_5ax\postprocessor\heidenhaintnc_PostConfigurator\sim08_mill_5ax_tnc)

 

I want to make it through the existing Post Builder.

 

However, Even if main mcs and local mcs are the same, DATUM SHIFT block is always output. (ref:MACH\resource\library\machine\installed_machines\sim08_mill_5ax\postprocessor\heidenhaintnc_PostConfigurator\sim08_mill_5ax_tnc_mm)

 

Where is the setting wrong?

5 REPLIES 5

Re: [Post Builder] DATUM SHIFT

Legend
Legend

Some explanations.

 

The MCS with Purpose MAIN is only used if there is no machine loaded.

Otherwise the "Machine Zero" Junction is used for Machine reference zero point.

 

You can adjust the output of the Zero Offset in PC as you like.

If you want no Output of Zerro Offset switch it to off.

27-06-_2018_09-02-34.png

 

Regards

Re: [Post Builder] DATUM SHIFT

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

Thank you

 

However, I do not use post configurator.

I want to set it through Post Builder.

Re: [Post Builder] DATUM SHIFT

Phenom
Phenom

Try using CSYS Rotation on the part work offset. It usually outputs a transformation. 

 

 

csys rotation.PNG

Glenn Balon
Production: NX 12.0.2 MP10 Primarily CAM

Re: [Post Builder] DATUM SHIFT

Legend
Legend

Which Postprocessor you use?

 

Controller?

Re: [Post Builder] DATUM SHIFT

Phenom
Phenom

See this link in docs too:

 

https://docs.plm.automation.siemens.com/tdoc/nx/12.0.1/nx_help/#uidSmiley Tonguearent_groups_parent_group_mcs

 

 

 

It outputs this transformation in the "out of the box" Siemens post. 

 

It should work on the Heidenhain posts form the machine sim as well. 

 

N450 ;
N460 ORIWKS
N470 ORIAXES
N480 G0 C0.0 A0.0
N490 TRANS X.3 Y.65 Z.5  <<<<<<<<<<<<<<<<<<<<<<

N500 G0 X.926921 Y1.678 Z8.8526 S0 D60 M3
N510 ;Approach Move
N520 Z4.9376
N530 ;Engage Move

 

post pic.PNG


csys offset.PNG

Glenn Balon
Production: NX 12.0.2 MP10 Primarily CAM

Learn online





Solution Information