Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Post Builder-Hole Making

Pioneer
Pioneer

Request for assistance, thanks...

 

Controller: Fanuc

 

Question 1: How to define Unclamp / clamp, in hole making?

 Q1.jpg

 

Question 2:When non cutting moves set clearance option: cylinder, only output this

 

Q2.jpg

15 REPLIES 15

Re: Post Builder-Hole Making

Legend
Legend

Hi,
1) Add unclamp/clamp before/after any rotation in the postprocessor.
2) To get rid of too many rotary moves, use the procedures from Postbuilder library (POSTBUILD\pblib\custom_command\pb_cmd_combine_rotary.tcl) in the postprocessor.

Re: Post Builder-Hole Making

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

RE: unclamp/clamp

Do you have "auto" clamping turned on in the post (or in UDE?)?

Before changing anything in the post, add a "Clamp" UDE,. set "Clamp Axis" to "Auto"

See what comes out.

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Post Builder-Hole Making

Pioneer
Pioneer
Dear Ken

Thank you so much.

Re: Post Builder-Hole Making

Pioneer
Pioneer

Hi,FROBI

Thank you so mach.
How should I use this?
(pb_cmd_combine_rotary.tcl)

I don't know tcl

Re: Post Builder-Hole Making

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

RE: Combine rotary

Open the post in post builder

"program and toolpath" tab -> "Custom commands" tab

"Import" button

navigate to your NX install folder, then \POSTBUILD\pblib\custom_command

select "pb_cmd_combine_rotary.tcl" -> Open

Note the 3 PB_CMD_* procedures it is adding - note their names down (or remember they all start with "PB_CMD__combine_")

"OK" to add the 3 procedures

Find them in the list of custom commands - read the comments at the top of each and follow the instructions

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Post Builder-Hole Making

Pioneer
Pioneer

Hi,Ken

 

Thanks for your reply.

What should I do?Please help

0.jpg

1.jpg2.jpg3.jpg

Re: Post Builder-Hole Making

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Create a new custom command PB_CMD_before motion.

Add the call to (whatever) to it.

 

You don't need to add PB_CMD_before motion to any event - if it exists, UGPost will call it at the appropriate places

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Post Builder-Hole Making

Pioneer
Pioneer

Hi,Ken

 

Thank you so much,problem solved.Smiley Happy

Re: Post Builder-Hole Making

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello Ken,

You do not know how this problem with a listing of the rotary axis to resolve the Postconfigurator?

Thanks Paul

Learn online





Solution Information