Cancel
Showing results for 
Search instead for 
Did you mean: 

Post Builder - How/where to change the NC init string

Legend
Legend

Can't seem to be able to figure out how (and where) to change in the post the BRISK and G60 modes. Where does the post get that from? From a UDE? built-in/static?

 

I had a look at the *.TCL under proc MOM_start_of_program { } but can't figure this out on my own. Any insight or help would be appreciated guys.

 

Also, how to change the language to English (less of a problem, but would be nice anyway).

 

TIA for any help guys

(NX 12)

 

PB-BRISK.jpg

5 REPLIES

Re: Post Builder - How/where to change the NC init string

Valued Contributor
Valued Contributor

Could you please send more detailed information, what do you have in the "start of program" tab in Post Builder?

If post output it, it definitely should be there.

Re: Post Builder - How/where to change the NC init string

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello CWilson,

 

first sorry for the German text, that is fixed already and translated to be always English.

 

Now to you question:

You are refer to the group calls "State Attributes". That data is defined and filled from the Simulation driver. It has nothing to do with the post, that why you didn't find it in the TCL. Inside the CCF file of the controller it is possible to update different machine states and display them in this group. That data comes from the NC code only.

 

Hope that clarifies it

Thomas

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: Post Builder - How/where to change the NC init string

Valued Contributor
Valued Contributor

Hello SpaceTom,

 

It is not totally clear for me. I define the initial machine state for each channel in INI files.

So the internal veriables - "State attribute" also define it? 

And how correctly work with them?

 

Thank you very much for your cooperation.

 

Re: Post Builder - How/where to change the NC init string

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

each StateAttribute can have an inital value. You can see it inside the Machine Configurator StateAttributes-inMC.png

 

Such Attributes are updated based on the NC Code. e.g. G60 will set that value to G60 G601

 

Hope that helps

Thomas

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: Post Builder - How/where to change the NC init string

Valued Contributor
Valued Contributor

Thank you so much for your respond. It clarifies a lot.

 

Kind Regards,

Nataliia.

Learn online





Solution Information