Cancel
Showing results for 
Search instead for 
Did you mean: 

[Post Builder] K Code is "ZERO" in Workplane code(G68.2)

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

Hi

 

setting a post builder.

 

# Infomatation

1. Machine Type : 5_axis_head_table (BC)

2. NX Version : NX10

3. Image :

 

Machine.jpg

4. CALCULATE_ANGLE "ZXZ"

5. Request : K code is alway "0" in G68.2 Code Blcok.

 

When the value of 0 is forcibly set, the XY coordinate value is wrong.

Where do I set it up? please help me.

 

 

 

Learn online





Solution Information