Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

[Post Builder] Multichannel machine Sim 15. Change the name of the program file

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi everybody,

 

How can I change the name of the program file. I'm use Sim15 fanuc multichannel

For example, if I output NC program from one channel I can change name of the program file. But, if I output NC program from synchronization module I can't change names program files. I need the program to be called the same as the file.(for example program name: O0010; file name O0010.NC)

 

Learn online





Solution Information