Cancel
Showing results for 
Search instead for 
Did you mean: 

[Post Builder] Rotational position change

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

Hi

 

I created a process using a Grinder (T-Cutter) tool.
 
TEST.jpg
 
Lock is set to rotate A aixs.
 
However, the starting point starts at the bottom due to the negative Y coordinate.
I want to rotate the A axis so that the Y axis is output as a positive value.
 
How do I change it?
 
 

 

2 REPLIES 2

Re: [Post Builder] Rotational position change

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Before the lock axis, try a ROTATE UDE

I would start with the options set to

- Aaxis

- Absolute

- None

- Rotation angle = 180 (or -180)

- Reference Only - No Output = "checked"

 

Make sure it is BEFORE the "lock axis" UDE

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: [Post Builder] Rotational position change

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

Hi Ken_A

 

I set up Lock Axis and rotate.

 

UDE.jpg

 

However, the Z value changes together and is output as the value of the wrong position.
 
ISV.jpg
 
How can we solve it? Thank you...

Learn online





Solution Information