Cancel
Showing results for 
Search instead for 
Did you mean: 

Post Builder: Start and End angles of an arc

Pioneer
Pioneer

Does anyone know how to get the start and end angle of an arc?

 

 

Ron

NX10.0.3

Windows 7 

2 REPLIES 2

Re: Post Builder: Start and End angles of an arc

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

No exist mom_vars for start angle and end angle of arc. For planar cases you can calc angles, you have info for arc center, start point, and arc angle or end point.

Re: Post Builder: Start and End angles of an arc

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Note there is mom_arc_angle which is the included angle of the arc, so once you get the start, you can use this to calculate the end.

Or else use it to double-check your calculations

 

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information