Cancel
Showing results for 
Search instead for 
Did you mean: 

[Post Builder] TRANS position value

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

Hi

 

I am building a post builder with the following information.

 

## Information

1. Machine type : Horizontal BC Table-Table type

2. Controller : SIEMENS 840D

3. Question

 

I have a problem with the current TRANS output value.

Currently, the TRANS value is output only from the origin to the TRANS point regardless of the rotation.

 

55.jpg

 

Even if the initial rotation axis is changed, it is not reflected.

And this equipment does not use AROT.

 

77.jpg

 

 

 

I would like to change the TRANS value according to the rotation as below.

 

66.jpg

 

 

Please give me a lot of advice.

3 REPLIES 3

Re: [Post Builder] TRANS position value

Legend
Legend
Hello

if you use PostConfigurator you need to switch off CYCLE800 Output and enable TRANS/ROT.
Then you are done.

Re: [Post Builder] TRANS position value

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator
Hi~

I did not use PostConfigurator, I used post builder and this machine does not use CYCLE800.
I want to set the desired value to output TRANS X460 Y0 Z-270.5.

Re: [Post Builder] TRANS position value

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Does this value change, or is it always the same?

Do you want it output output once @ start of program, or at every tool change?

 

One option is to define a couple expressions (could be defined as measurments) with the desired values.  (e.g. TRANS_ORIGIN_X and TRANS_ORIGIN_Y)

 

Then in your post:

- if expression doesn't exist, don't output value (e.g. if X doesn't exist, just output "TRANS Ynnn")

- if expression exists , output that value

 

If you need multiple, you can use multiple expressions ("TRANS_ORIGIN_X_1") based on whatever index you need (if different MCS, you could use fixture offset.  Or you could use a UDE to specify which index to use.  Or whatever)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information