Cancel
Showing results for 
Search instead for 
Did you mean: 

[Post Builder] TRANS position

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

Hi

 

##

1. Controller : SIEMENS 840D

2. TYPE : Holizontal-Table-Table-BC Type

3. Version : NX11.0.2

4. Request :

 

I have to modify the TRANS code.

 

If the B axis has a value that rotates 90 degrees.

The TRANS ZERO value is X460 Z270.5.

However, when the post process is executed, the following values are output.

11.jpg

 

Where can I get normal values to fix?
Thank you for your advice.

 

22.jpg

 

 

 As a result, the XYZ value of the CSYS Rotation coordinate is output from the Main coordinate reference. The problem is that coordinate values that ignore the rotation value are being output.

Learn online





Solution Information