Cancel
Showing results for 
Search instead for 
Did you mean: 

[Post Builder] check motion resolution

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

Hi

 

I try post Builder.

When you save or open the settings, the following window will be activated.

 

Format setting may not accommodate the output for "Rotary Motion Resolution".

TEST.jpg

 

What is the cause and how should I fix it?

4 REPLIES

Re: [Post Builder] check motion resolution

Legend
Legend

You have to check some parameters.

In PB check which Format is used for X,Y,Z

 27-06-_2018_08-10-29.png

Then look how many decimals this format have you can use the edit button

27-06-_2018_08-17-30.png

 

Then you have to set the Linear Motion Resolution and the Rotary Motion Resolution to a smaller Value

27-06-_2018_08-22-43.png

 

27-06-_2018_08-24-23.png 

 

Thats it

 

Re: [Post Builder] check motion resolution

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I've found that if they aren't EQUAL (the format & resolution) you get the warning.

One way around this is to set them equal in those dialogs, then add a custom command (in "start of prorgam") something like:

global mom_kin_4th_axis_min_incr  
global mom_kin_5th_axis_min_incr 
global mom_kin_machine_resolution 
  set mom_kin_4th_axis_min_incr                 "0.0001"
  set mom_kin_5th_axis_min_incr                 "0.0001"
  set mom_kin_machine_resolution                ".000001"

MOM_reload_kinematics

Use values appropriate to you.

 

The only problem with this is that these settings are "hidden" (not set in the "normal" place) so other users who try to edit your post may have a problem figuring out where you set them

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Highlighted

Re: [Post Builder] check motion resolution

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you need different resolutions, just add another format, like rotary_coordinate, and assign it to the rotary axis.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: [Post Builder] check motion resolution

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

Thank you everyone.

 

It has been resolved.

 

 

Learn online





Solution Information