Cancel
Showing results for 
Search instead for 
Did you mean: 

Post Builder output.

Creator
Creator

I run 5axis Post-Processor /4+1/, and receave strenge output.

What it can be?

 

N0076 PX = -14.38800099249092000 CX = -14.38800099249092000

N0086 PY = -0.65000000095440169 CY = -0.57000099287970929

N0096 PZ = 0.88800000000000068 CZ = 0.88800000000000057

N0106 NX = -14.65902511247981900 CX = -14.38800099249092000

N0116 NY = -0.57000099287970929 CY = -0.57000099287970929

N0126 NZ = 0.88800000000000057 CZ = 0.88800000000000057

N0136 P4 = -0.00000000000000000 C4 = -0.00000000000000000

6 REPLIES

Re: Post Builder output.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Assuming you mean the number of decimal places output is extreme...

 

Looks like someone is directly outputting values, rather than using a block template.

e.g.

MOM_output_literal PX=$variable1 CX=$variable2

instead of

 

MOM_do_template your_block_name

If you do the first, you can add code like this before the MOM_output_literal, to format the data

 

set v1_out [string trimright [format "%.4f" $variable1] "0"]
set v2_out [string trimright [format "%.4f" $variable2] "0"]

MOM_output_literal PX=$v1_out CX=$v2_out

But it would probably be better to define words & blocks & let Post Builder do the formatting for you.

 

 

The other option is someone defined the formats used by those words to 17 or whatever decimal places (if that is possible?)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Post Builder output.

Creator
Creator

Hello Ken.

Thank You for timle and deteiled respond, I try to fined, wher this MOM_output_lliteral...., to chenge on MOM_do_template your_block_name,wher You think this can be?

Re: Post Builder output.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

In the "Post process" dialog, turn on the review tool

In the resulting TK dialog, in the right column, click on one of the lines with the output you want to change

This will select (in the left column) the event generating that line.

 

Then you'll have to look at that event in Post Builder to see what they are doing (probably calling a "PB_CMD_...").

 

Ken

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Post Builder output.

Creator
Creator

Hello Ken.

Finde, Comand : PB_CMD__combine_rotary_check.

Try to turn it off.

Re: Post Builder output.

Siemens Legend Siemens Legend
Siemens Legend

If you re-import the PB_CMD__combine_rotary_xxx commands from the newer PB, the numbers output would be rounded to the output resolutions.

 

Re: Post Builder output.

Creator
Creator

Hello Postino.

Thank You for waluble input, I will

use this nex time, I am going to run this Post-Processor.

Thank You for Your time, Sir.

Learn online





Solution Information