Cancel
Showing results for 
Search instead for 
Did you mean: 

Post Builder + "Advanced turbo mode" + "Synchronization Manager" = True?

Experimenter
Experimenter

Hi,

 

I´m currently updating some posts with activating the "Advanced turbo mode" to improve the performance.

Now i´m a bit stuck with a multiple channel machine.

I cant find any information if "Advanced Turbo mode" is possible together with Sync. manager...

 

if it's not possible, is it doable with a post created from "Post configurator"?

 

 

My current versions

NX 12.0.1.7

PB 12.0.1

 

Regards

Henrik

 

 

 

 

 

2 REPLIES

Re: Post Builder + "Advanced turbo mode" + "Synchronization Manager" = True?

Siemens Legend Siemens Legend
Siemens Legend

Hi Henrik,

 

the advanced turbo mode is supported in ISV & Sync manager simulation since NX12.0.1. For PB Just implement the custom commands from NX help and following the instructions documented in each custom command.

 

If you want to use Post Configurator it's not needed to do some customization because this is a OOTB feature of Post Configurator, just switch on the Turbo mode property.

 

Best regards

Thomas

Re: Post Builder + "Advanced turbo mode" + "Synchronization Manager" = True?

Experimenter
Experimenter
Hi Thomas

Thanks for the reply!
It's good to know that it should work. In that case i know that i'm doing something wrong.
I'll get errors like "Missing turbo-xxxx block templates" when i start sync.manager and the post runs fine outside it...

I'll get back if i don't succeed with your recommendations=)
Regards
Henrik

Learn online





Solution Information