Cancel
Showing results for 
Search instead for 
Did you mean: 

Post Builder

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi Guys!

 

Good Day, where can i get a post builder for NX10?

Thanks

7 REPLIES

Re: Post Builder

Valued Contributor
Valued Contributor

If your talking about the program it is installed with NX. It can be found in start menu in the siemens folder under the manufacturing folder. It should point to this file here  C:\Program Files\Siemens\NX 8.0\POSTBUILD\post_builder.ba

 

If your talking about the actual post files then NX comes with standard ones. If you want anymore then you can download some from Siemens, Pay for them or Create you own.

Using NX 8.0.3.4

Re: Post Builder

Like @aluminum2 says, Post Builder is part of NX, so it's on your system :*). 

Is there something in particular you are looking for?

Mark Rief
Retired Siemens

Re: Post Builder

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Or are you saying it is broke and you would like one that actually works?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Post Builder

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi Guys, Thanks for the help, already found it. Have a good day!!!

Re: Post Builder

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

hahaha, when i try to create new post, it will come out with error.

Re: Post Builder

Phenom
Phenom

See Mark's comment in a couple threads down:

 

http://community.plm.automation.siemens.com/t5/Discussion-Forum-NX/10-0-3-5-Post-Builder-Auto-Clamp/...

NX12.02
Windows 10 Pro

Re: Post Builder


@Azrul wrote:

hahaha, when i try to create new post, it will come out with error.


Like @Study says, please update your system.

The image shows Postbuilder 10, which was released in 2014.

Mark Rief
Retired Siemens

Learn online





Solution Information